How to load i.MX8M DDR tool by u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to load i.MX8M DDR tool by u-boot?

Jump to solution
1,383 Views
m_c
Senior Contributor I
0 Kudos
Reply
1 Solution
1,184 Views
art
NXP Employee
NXP Employee

There is no way to load the i.MX8M DDR tool by u-boot, as it was possible with the i.MX6/7 DDR Stress Test Tool. Only the Windows-based GUI option of the i.MX8M DDR tool is available.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,185 Views
art
NXP Employee
NXP Employee

There is no way to load the i.MX8M DDR tool by u-boot, as it was possible with the i.MX6/7 DDR Stress Test Tool. Only the Windows-based GUI option of the i.MX8M DDR tool is available.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply