How to load and install module automatically at kernel bootup in standalone build?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to load and install module automatically at kernel bootup in standalone build?

跳至解决方案
2,440 次查看
RVT
Contributor I

Hello, NXP experts:

By using demo files (LF_v6.1.1_1.0.0_images_IMX8MPEVK or LF_v5.15.71-2.2.0_images_IMX8MPEVK) from "https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...", all peripherals can be found and loaded properly on i.MX 8M Plus EVK.

For example, WM8960 can be found with demo files.

RVT_0-1684469111192.png

But there is no peripherals found by using the standalone built image with "https://github.com/nxp-imx/linux-imx". The default "imx_v8_defconfig" and "imx8mp-evk.dts" are applied in the build.

For example, no soundcard can be found with standalone built kernel image.

RVT_1-1684469163893.png

 

How can I build the same kernel image as the demo files?

Thanks.

0 项奖励
回复
1 解答
2,330 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @RVT,

I hope you are doing well.

Please make sure that snd-soc-fsl-asoc-card.ko module is loaded correctly.

One can try building a linux image using yocto.

Please refer to i.MX Yocto Project User's Guide

One can refer to the below-mentioned documents related to Audio Codec porting.

1. Chapter 7 Audio - i.MX Linux Reference Manual

2. Chapter - 16 Porting Audio Codecs in i.MX Porting Guide

3 . Audio Codec WM8960 Porting Notes

4. WM8960 audio codec

5. Porting custom audio codec in Linux BSP

Thanks & Regards,
Dhruvit Vasavada

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,399 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @RVT,

I hope you are doing well.

One needs to enable menuconfig options in the kernel to load specific modules.

Please refer to 7.1.4.6 Menu Configuration Options in i.MX Linux Reference Manual to enable SoC Audio supports for WM8958, WM8960, and WM8962 CODEC.

One can add module names in /etc/modules-load.d/<module_list>.conf to automatically load kernel modules.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复
2,364 次查看
RVT
Contributor I

Hi Dhruvit,

Attached please find the .config & imx_v8_defconfig files at iMX Linux kernel at https://github.com/nxp-imx/linux-imx.

There is no option for wm8960 as shown in 7.1.4.6.

RVT_2-1685091435048.png

 

RVT_1-1685091211794.png

 

RVT_0-1685090998095.png

I intend to port another codec to EVK platform by following the baseline EVK kernel code. Therefore, I would like to know all know-how in order to let a new codec to work with iMX8MP SAI and audio framework. Firstly, I have to build the same as the demo files. 

Also, can NXP provide something like audio subsystem linux porting guide - user manual?

Thanks.

标记 (1)
0 项奖励
回复
2,331 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @RVT,

I hope you are doing well.

Please make sure that snd-soc-fsl-asoc-card.ko module is loaded correctly.

One can try building a linux image using yocto.

Please refer to i.MX Yocto Project User's Guide

One can refer to the below-mentioned documents related to Audio Codec porting.

1. Chapter 7 Audio - i.MX Linux Reference Manual

2. Chapter - 16 Porting Audio Codecs in i.MX Porting Guide

3 . Audio Codec WM8960 Porting Notes

4. WM8960 audio codec

5. Porting custom audio codec in Linux BSP

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复