How to load a compiled C application on 8mPLUS EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to load a compiled C application on 8mPLUS EVK

1,345 次查看
ShivM
Contributor II

Hi,

I have compiled a C Application for IMX 8M PLUS EVK.

Now I want to load the C application on IMX 8M PLUS EVK.. Not the entire boot image..

I searched UUU it has instructions to load the boot image but not just a regular application image

0 项奖励
回复
3 回复数

1,341 次查看
Yuri
NXP Employee
NXP Employee

@ShivM 
Hello,

   You may try to use WinSCP.

Regards,
Yuri.

0 项奖励
回复

1,335 次查看
ShivM
Contributor II

Hi Yuri,

 

I tried using.. Is there any documentation what should be the IP address of Host?

I used to load other(no nxp) boards using WinSCP and would like to do that. I will need the IP addresses of Host PC.

0 项奖励
回复

1,329 次查看
Yuri
NXP Employee
NXP Employee

 You need IP address of the target board. Its IP can be received, using DNS or configured 
manually.

 

~Yuri.

0 项奖励
回复