How to interrupt i.MX28 MfgTool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to interrupt i.MX28 MfgTool?

跳至解决方案
1,162 次查看
m_c
Senior Contributor I

Is there anyway to interrupt MfgTool while update firmware?

For example, detect checksum of firmware is wrong.

标签 (2)
0 项奖励
回复
1 解答
1,078 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

there is no special crc checking in mfg tools, if necessary one can try to

customize it using sources:

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL_SOURCE  : Source Code for the i.MX manufacturing tool used
for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23..
Size (K): 1226 Format: zip Rev #: 1.6.2.055 Modified: 7/22/2013

i.MX53 Quick Start Board | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,079 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

there is no special crc checking in mfg tools, if necessary one can try to

customize it using sources:

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL_SOURCE  : Source Code for the i.MX manufacturing tool used
for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23..
Size (K): 1226 Format: zip Rev #: 1.6.2.055 Modified: 7/22/2013

i.MX53 Quick Start Board | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复