How to interrupt i.MX28 MfgTool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to interrupt i.MX28 MfgTool?

Jump to solution
1,157 Views
m_c
Senior Contributor I

Is there anyway to interrupt MfgTool while update firmware?

For example, detect checksum of firmware is wrong.

Labels (2)
0 Kudos
Reply
1 Solution
1,073 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

there is no special crc checking in mfg tools, if necessary one can try to

customize it using sources:

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL_SOURCE  : Source Code for the i.MX manufacturing tool used
for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23..
Size (K): 1226 Format: zip Rev #: 1.6.2.055 Modified: 7/22/2013

i.MX53 Quick Start Board | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,074 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

there is no special crc checking in mfg tools, if necessary one can try to

customize it using sources:

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL_SOURCE  : Source Code for the i.MX manufacturing tool used
for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23..
Size (K): 1226 Format: zip Rev #: 1.6.2.055 Modified: 7/22/2013

i.MX53 Quick Start Board | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply