How to interface freescale K81 with i.MX6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface freescale K81 with i.MX6?

1,468件の閲覧回数
hrushinale
Contributor III

Hello Community,

For one of my application it requires to interface freescale K81 MCU with i.MX6 over SPI interface.

Do I need to write the driver for communication between these devices ?

If yes then please suggest some driver names for reference.

Thanks & Regards,

Hrushi

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

1,361件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

one can try to adapt imx-test (folder /mxc_spi_test)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

just for reference one can also look at attached Linux Manual

Chapter 31 SPI NOR Flash Memory Technology Device (MTD) Driver

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信