How to interface USB HSIC on iMX8QM in devicetree?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface USB HSIC on iMX8QM in devicetree?

ソリューションへジャンプ
3,335件の閲覧回数
philippe_schenk
Contributor IV

Hello

On L4.14 releases there has always been a device-tree-node called &usbh1 (@ 0x5b0e0000) with that we were able to interface the USB HSIC interface to our USB Hub.

In the latest L5.4.24-2.1.0 release there is no such interface anymore. I searched with the address (0x5b0e0000) if it is newly named but was not successful. This interface seems to be completely gone.

I then tried to bring up the usb interface with fsl,imx7ulp-usb compatible but without success. It always crashed when trying to load so I gave up.

Our original question from 2.5 years ago was here: USB HSIC support for iMX8QM

This issue seems to be tracked in your internal system as: MLK-16715

Could you please send us a patch where you add support back for interface 0x5b0e0000 on iMX8QM (pads USB_HSIC0_STROBE and USB_HSIC0_DATA)

Thanks in advance,
Philippe Schenker

cc: PeterChen 

ラベル(1)
タグ(3)
1 解決策
3,294件の閲覧回数
PeterChen
NXP Employee
NXP Employee

Hi Philippe,

Tried to add attached two patches, and see if your problem is fixed.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,284件の閲覧回数
philippe_schenk
Contributor IV

Thank you very much, this patches work well!

0 件の賞賛
返信
3,295件の閲覧回数
PeterChen
NXP Employee
NXP Employee

Hi Philippe,

Tried to add attached two patches, and see if your problem is fixed.

0 件の賞賛
返信