How to interface 18-bit lcd with i.MX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to interface 18-bit lcd with i.MX6ULL

4,042 次查看
Gallopwc
Contributor I

I am trying to interface 18-bit lcd with i.MX6ULL. According to the user manual, data pins used in 18-bit DOTCLK mode is LCD_DATA00 - LCD_DATA17, so I connect the display like this:

LCD_DATA00 ------ B0

LCD_DATA01 ------ B1

LCD_DATA02 ------ B2

LCD_DATA03 ------ B3

LCD_DATA04 ------ B4

LCD_DATA05 ------ B5

LCD_DATA06 ------ G0

LCD_DATA07 ------ G1

LCD_DATA08 ------ G2

LCD_DATA09 ------ G3

LCD_DATA10 ------ G4

LCD_DATA11 ------ G5

LCD_DATA12 ------ R0

LCD_DATA13 ------ R1

LCD_DATA14 ------ R2

LCD_DATA15 ------ R3

LCD_DATA16 ------ R4

LCD_DATA17 ------ R5

 

The kernel version used is 4.1.15, and my DTS is as follow

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
status = "okay";

display0: display {
bits-per-pixel = <32>;
bus-width = <18>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <6300000>;
hactive = <320>;
vactive = <240>;
hfront-porch = <65>;
hback-porch = <10>;
hsync-len = <5>;
vback-porch = <7>;
vfront-porch = <12>;
vsync-len = <3>;

de-active = <1>;
hsync-active = <0>;
vsync-active = <0>;
pixelclk-active = <0>;
};
};
};
};

But pictures are not display in right color, there seems to be a lack of green, I have shown a QT routine (animatedtiles) on the screen, it is supposed to be dark green, but now it's dark red. The boot information on the screen should be white, but now it's blue. Images are clear except for the color. I don't know if the connection to the display is not right, or there is something wrong with my dts configuration.

0 项奖励
回复
4 回复数

3,999 次查看
Gallopwc
Contributor I

Thanks for your reply, @Sanket_Parekh .

Sure, I have attached the datasheet and the picture showed on my display.  As you can see, original qt example is dark green, but it's dark red on my display.

Thanks & Regards

Gallopwc

0 项奖励
回复

3,968 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

the R pins should be connected to the most significant bits, then G and finally B.

So for this 18-bit RGB LCD:

R[5:0] <-> LCD_D[21:16]

G[5:0] <-> LCD_D[13:08]

B[5:0] <-> LCD_D[05:00]

Thanks & Regards

Sanket Parekh

0 项奖励
回复

4,008 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

I hope you are doing well.

Can you please share the datasheet of the display to debug this issue further?

Thanks & Regards

Sanket Parekh

0 项奖励
回复

4,005 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

Waiting for your answer.

Thanks & Regards

Sanket Parekh

0 项奖励
回复