How to interface 18-bit lcd with i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to interface 18-bit lcd with i.MX6ULL

4,030 Views
Gallopwc
Contributor I

I am trying to interface 18-bit lcd with i.MX6ULL. According to the user manual, data pins used in 18-bit DOTCLK mode is LCD_DATA00 - LCD_DATA17, so I connect the display like this:

LCD_DATA00 ------ B0

LCD_DATA01 ------ B1

LCD_DATA02 ------ B2

LCD_DATA03 ------ B3

LCD_DATA04 ------ B4

LCD_DATA05 ------ B5

LCD_DATA06 ------ G0

LCD_DATA07 ------ G1

LCD_DATA08 ------ G2

LCD_DATA09 ------ G3

LCD_DATA10 ------ G4

LCD_DATA11 ------ G5

LCD_DATA12 ------ R0

LCD_DATA13 ------ R1

LCD_DATA14 ------ R2

LCD_DATA15 ------ R3

LCD_DATA16 ------ R4

LCD_DATA17 ------ R5

 

The kernel version used is 4.1.15, and my DTS is as follow

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
status = "okay";

display0: display {
bits-per-pixel = <32>;
bus-width = <18>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <6300000>;
hactive = <320>;
vactive = <240>;
hfront-porch = <65>;
hback-porch = <10>;
hsync-len = <5>;
vback-porch = <7>;
vfront-porch = <12>;
vsync-len = <3>;

de-active = <1>;
hsync-active = <0>;
vsync-active = <0>;
pixelclk-active = <0>;
};
};
};
};

But pictures are not display in right color, there seems to be a lack of green, I have shown a QT routine (animatedtiles) on the screen, it is supposed to be dark green, but now it's dark red. The boot information on the screen should be white, but now it's blue. Images are clear except for the color. I don't know if the connection to the display is not right, or there is something wrong with my dts configuration.

0 Kudos
Reply
4 Replies

3,987 Views
Gallopwc
Contributor I

Thanks for your reply, @Sanket_Parekh .

Sure, I have attached the datasheet and the picture showed on my display.  As you can see, original qt example is dark green, but it's dark red on my display.

Thanks & Regards

Gallopwc

0 Kudos
Reply

3,956 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

the R pins should be connected to the most significant bits, then G and finally B.

So for this 18-bit RGB LCD:

R[5:0] <-> LCD_D[21:16]

G[5:0] <-> LCD_D[13:08]

B[5:0] <-> LCD_D[05:00]

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

3,996 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

I hope you are doing well.

Can you please share the datasheet of the display to debug this issue further?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

3,993 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Gallopwc 

Waiting for your answer.

Thanks & Regards

Sanket Parekh

0 Kudos
Reply