How to improve the received Video Frame rate on a network using gstreamer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to improve the received Video Frame rate on a network using gstreamer

1,639 Views
santhosh2
Contributor IV

I am doing a multicast streaming using RTP and the framerate is set to 30fps but i am receiving only 13 frames at the receiver end. How can i improve this

Transmitter command gst-launch-1.0 v4l2src device=/dev/video0 ! tee name=t ! queue ! videoscale ! 'video/x-raw,width=640,height=480, framerate=(fraction)30/1' ! videoconvert ! queue2 ! x264enc tune=zerolatency ! rtph264pay ! multiudpsink auto-multicast=true send-duplicates = true bind-port=5000 clients="255.255.255.255:5000"

Receiver command gst-launch-1.0 udpsrc port=5000 ! application/x-rtp,encoding-name=H264 ! rtpjitterbuffer ! rtph264depay ! avdec_h264 ! videoconvert ! fpsdisplaysink sync=true -v

framerate.png

0 Kudos
Reply
4 Replies

1,505 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

for RTP one can look at sect.7.3.12 Real Time Streaming Protocol Linux Guide

in Linux 4.19.35_1.1.0 Documentation

and some examples on DART-MX8M GSTREAMER - Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,505 Views
santhosh2
Contributor IV

Hi igorpadykov,

Thanks for the links, I tried with the link that you have shared using the num-buffers=100 but still at the receiver end i am not seeing the 30fps, only 14fps are received. How can i get max frames transmitted without any lose at the receiver end

Looking forward for your support on this...

Regards

Santhosh

0 Kudos
Reply

1,505 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

 

please try Demo Images with NXP reference board

i.MX Software and Development Tools | NXP 

 

Best regards
igor

0 Kudos
Reply

1,505 Views
santhosh2
Contributor IV

Hi igor,

Iam using the same image with NXP Eval board. The problem still persist

Regards

Santhosh

0 Kudos
Reply