How to get output from mfgtool command line interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get output from mfgtool command line interface?

1,800 次查看
raymatlin
Contributor I

I am using mfgTool2 from the command line with the -noui parameter. It downloads the firmware fine but there is no output in the cmd window. I am using this in a production environment in a C# program. I would like to be able to display the kinds of progress you see when mfgTool2 is run as a GUI.

0 项奖励
回复
1 回复

1,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ray

available options are described in Quick Start Guide p.8, also one

can customize for own needs using sources

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复