How to get output from mfgtool command line interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get output from mfgtool command line interface?

2,418件の閲覧回数
raymatlin
Contributor I

I am using mfgTool2 from the command line with the -noui parameter. It downloads the firmware fine but there is no output in the cmd window. I am using this in a production environment in a C# program. I would like to be able to display the kinds of progress you see when mfgTool2 is run as a GUI.

0 件の賞賛
返信
1 返信

2,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ray

available options are described in Quick Start Guide p.8, also one

can customize for own needs using sources

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信