How to fully secure an IMX8M device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fully secure an IMX8M device

582 Views
TomHarvey
Contributor II

Hi all, 

I am currently trying to fully secure an IMX8M device. I have programmed the SRK_HASH and am currently able to perform a high assurance boot with a signed bootloader and image.

In the AN4581 it lists the following fuses that must be programmed to fully secure the device:

• SRK_LOCK: Lock for SRK_HASH[255:0] fuses.
• DIR_BT_DIS: Disable direct external memory boot.
• SJC_DISABLE: Disable the secure JTAG controller module.
• JTAG_SMODE: Set JTAG security mode to no debug mode 0x11.
• JTAG_HEO: Disallows HAB JTAG enabling.
• BOOT_CFG_LOCK: Lock on BOOT related fuses.

I have worked out the the word, bank and fuse values by reading IMX8MDQLQRM and IMX8MDQLQSRM for the SRK_LOCK, BOOT_CFG_LOCK and SEC_CONFIG: (Please let me know if these are correct).

SRK_LOCK

fuse prog 0 0 0x100

BOOT_CFG_LOCK

fuse prog 0 0 0xC

SEC_CONFIG

fuse prog 1 3 0x2000000


For DIR_BT_DIS the technical specification states that:

"The DIR_BT_DIS eFuse must be programmed prior to shipping
a device in a security enabled configuration. If the this eFuse is
not blown, the system is not secure."

So I assume that this does not need to be programmed.

For SJC_DISABLE and JTAG_SMODE I cannot find the mappings in the technical specification and have come across a forum post that details the following:

Fuse addrFuse nameNum bitsFuse functionSettingUsed by
0x470[21]SJC_DISABLE1Disable/Enable the Secure JTAG Controller module. This fuse is used to create highest JTAG security level, where JTAG is totally blocked.0 - Secure JTAG Controller is enabled
1 - Secure JTAG Controller is disabled
SJC
0x470[23:22]JTAG_SMODE[1:0]2JTAG Security Mode. Controls the security mode of the JTAG debug interface00 - JTAG enable mode
01 - Secure JTAG mode
11 - No debug mode
SJC


https://community.nxp.com/t5/i-MX-Processors/DIR-BT-DIS-and-others/m-p/1212354 

And i can't see a mention of JTAG_HEO.

I would like to understand the following to fully secure the device:

 

  • Does DIR_BT_DIS need to be programmed? If so what values?
  • For SJC_DISABLE and JTAG_SMODE are the values shown in the table above 0x470[21] and 0x470[23:22] correct?
  • Do i need to program JTAG_HEO if so what is its fuse mapping?
  • Is there anything additional i need to program to fully secure the device. For instance do i need to program fuses such as FIELD_RETURN? 

Please may someone send the the relevant information or documents detailing this.

Kind regards, 

Tom

3 Replies

550 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Will reply back to you in system email as some fuse information can't be discussed publicly.

 

Regards

Harvey

0 Kudos
Reply

535 Views
emmanuel_madrigal
Contributor I

Hi Harvey,

 

Would it be possible for you to send me this information as well?

 

Regards,

Emmanuel

0 Kudos
Reply

501 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @emmanuel_madrigal 

As some information is under NDA, suggest to raise a ticket with Confidential assistance 

 

Regards

Harvey

0 Kudos
Reply