Hi all,
I am currently trying to fully secure an IMX8M device. I have programmed the SRK_HASH and am currently able to perform a high assurance boot with a signed bootloader and image.
In the AN4581 it lists the following fuses that must be programmed to fully secure the device:
• SRK_LOCK: Lock for SRK_HASH[255:0] fuses.
• DIR_BT_DIS: Disable direct external memory boot.
• SJC_DISABLE: Disable the secure JTAG controller module.
• JTAG_SMODE: Set JTAG security mode to no debug mode 0x11.
• JTAG_HEO: Disallows HAB JTAG enabling.
• BOOT_CFG_LOCK: Lock on BOOT related fuses.
I have worked out the the word, bank and fuse values by reading IMX8MDQLQRM and IMX8MDQLQSRM for the SRK_LOCK, BOOT_CFG_LOCK and SEC_CONFIG: (Please let me know if these are correct).
SRK_LOCK
fuse prog 0 0 0x100
BOOT_CFG_LOCK
fuse prog 0 0 0xC
SEC_CONFIG
fuse prog 1 3 0x2000000
For DIR_BT_DIS the technical specification states that:
"The DIR_BT_DIS eFuse must be programmed prior to shipping
a device in a security enabled configuration. If the this eFuse is
not blown, the system is not secure."
So I assume that this does not need to be programmed.
For SJC_DISABLE and JTAG_SMODE I cannot find the mappings in the technical specification and have come across a forum post that details the following:
Fuse addr | Fuse name | Num bits | Fuse function | Setting | Used by |
0x470[21] | SJC_DISABLE | 1 | Disable/Enable the Secure JTAG Controller module. This fuse is used to create highest JTAG security level, where JTAG is totally blocked. | 0 - Secure JTAG Controller is enabled 1 - Secure JTAG Controller is disabled | SJC |
0x470[23:22] | JTAG_SMODE[1:0] | 2 | JTAG Security Mode. Controls the security mode of the JTAG debug interface | 00 - JTAG enable mode 01 - Secure JTAG mode 11 - No debug mode | SJC |
https://community.nxp.com/t5/i-MX-Processors/DIR-BT-DIS-and-others/m-p/1212354
And i can't see a mention of JTAG_HEO.
I would like to understand the following to fully secure the device:
Please may someone send the the relevant information or documents detailing this.
Kind regards,
Tom
Hi Harvey,
Would it be possible for you to send me this information as well?
Regards,
Emmanuel
As some information is under NDA, suggest to raise a ticket with Confidential assistance
Regards
Harvey