How to flash OCOTP_MAC0/MAC1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to flash OCOTP_MAC0/MAC1

2,096 次查看
kalyankodamagul
Contributor I

I was looking to set fixed MAC address using the registers OCOTP_MAC0/MAC1 and read the configured MAC address.In the kernel code   freescale - 4.1.15   /drivers/net/ethernet/freescale/fec_main.c(fec_get_mac)  there are showing different options instead of using OCOTP method.Right now MAC address is randomly generated one.

 In i.MX 6Solo/6DualLite application processors 

Can someone guide us how to program below registers.

 21B_C620 (Absolute address) -Value of OTP Bank4 Word2 (MAC Address) (OCOTP_MAC0)

21B_C630(Absolute address)  - Value of OTP Bank4 Word3 (MAC Address) (OCOTP_MAC1)

And way to read these one.

-Thanks,

kalyan.

标签 (2)
0 项奖励
回复
1 回复

1,729 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following :

i.mx6 eFUSE Burning 

mx6 efuse 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复