How to fix IPU warning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to fix IPU warning

跳至解决方案
4,448 次查看
skappen
Contributor II

We are using a custom driver for capturing video (1280x722 YUV 422 @ 30fps) from two digital imagers on iMX6Q based custom board in freescale linux 3.10.17 kernel. One imager is connected to CSI0 port of first IPU and other connected to CSI1 port of second IPU. We are able to capture and verify the captured images. We are seeing the below ipu error interrupts  when multiple interrupts occur simultaneously in the system. For eg if we insert a usb disk to the system we are seeing  one or two IPU warnings for each insertion. I suspect this could be due to interrupt latency if so is there is any way to increase ipu interrupt priority? or any other method to avoid this frame lost situation?

IPU Warning - IPU_INT_STAT_10 = 0x00000002

IPU Warning - IPU_INT_STAT_10 = 0x00000001

标签 (4)
0 项奖励
回复
1 解答
3,744 次查看
skappen
Contributor II

The double buffer approach in IPU resolved the issue. In this scheme two buffers are initialized using the API ipu_init_channel_buffer() and kept ready for receiving frames.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,744 次查看
felixwei
Contributor I

Hi Sam,

I met the same issue, would you like to share how to fix it ?

0 项奖励
回复
3,745 次查看
skappen
Contributor II

The double buffer approach in IPU resolved the issue. In this scheme two buffers are initialized using the API ipu_init_channel_buffer() and kept ready for receiving frames.

0 项奖励
回复
3,744 次查看
Yuri
NXP Employee
NXP Employee

  Please look at the following :

Re: imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00000001


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,744 次查看
skappen
Contributor II

Thanks Yuri , I already gone through the links provided.  I am not getting continuous IPU Warning. The  IPU Warning - IPU_INT_STAT_10 = 0x00000001 seems to occur during time where multiple interrupts need to be serviced. IPU error interrupts frequency is around two/hour.    

0 项奖励
回复
3,744 次查看
Yuri
NXP Employee
NXP Employee

Perhaps the system is heavy loaded in Your case : VPU coding / encoding, USB, Ethernet

transfers, file storage. You may try to decrease system load.

Regards,

Yuri. 

0 项奖励
回复