Hi.
Which register should I set to enable core1 on i.MX7D?
Even if I set bit 2 of 6.2.7.3 A7 Reset Control Register in the Reference Manual to '1', there is no response.
Thank yoi.
解決済! 解決策の投稿を見る。
refer to the schematic, the pull-up is DNP, When JTAG_MOD is low, the JTAG interface is configured for common software debug,
元の投稿で解決策を見る
is it your typo? bit2 is for reserved, should be bit1
I'm sorry.
Bit 1 is correct.
The JTAG_MOD pin on the i.MX7D SABRE board is connected to a 10K pull-up register and a 4.7K pull-down register, but is the MPU in JTAG mode or SW mode?
Thank you.