Hi.
Which register should I set to enable core1 on i.MX7D?
Even if I set bit 2 of 6.2.7.3 A7 Reset Control Register in the Reference Manual to '1', there is no response.
Thank yoi.
Solved! Go to Solution.
refer to the schematic, the pull-up is DNP, When JTAG_MOD is low, the JTAG interface is configured for common software debug,
View solution in original post
is it your typo? bit2 is for reserved, should be bit1
I'm sorry.
Bit 1 is correct.
The JTAG_MOD pin on the i.MX7D SABRE board is connected to a 10K pull-up register and a 4.7K pull-down register, but is the MPU in JTAG mode or SW mode?
Thank you.