How to enable Wi-fi AR6103 in Sabre-AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Wi-fi AR6103 in Sabre-AI

Jump to solution
2,786 Views
nishad_kamdar
Contributor IV

Hello,

I have a custom iMx6Q board based on Sabre-AI. I need to interface the Atheros AR6103 to it in the SD2 slot.

I am using LTIB 3.0.35_4.1.0 _130816 BSP.

I wanted to know the procedure to enable the this Module in the Kernel.

Can anyone kindly help me in this regard....

Labels (2)
0 Kudos
Reply
1 Solution
1,687 Views
igorpadykov
NXP Employee
NXP Employee

Hi nishad

please look below

https://community.freescale.com/docs/DOC-94600

How to add Wi-Fi to Freescale i.MX 6 - YouTube

http://www.silexamerica.com/learning/app_notes/Freescale.pdf

All Boards Wi-Fi

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,688 Views
igorpadykov
NXP Employee
NXP Employee

Hi nishad

please look below

https://community.freescale.com/docs/DOC-94600

How to add Wi-Fi to Freescale i.MX 6 - YouTube

http://www.silexamerica.com/learning/app_notes/Freescale.pdf

All Boards Wi-Fi

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply