How to enable PCI-e interface for SABRESD with Linux rel_imx_3.10.17_1.0.2_ga?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enable PCI-e interface for SABRESD with Linux rel_imx_3.10.17_1.0.2_ga?

跳至解决方案
1,551 次查看
phanthavongdoua
NXP Employee
NXP Employee
0 项奖励
回复
1 解答
1,231 次查看
Yuri
NXP Employee
NXP Employee

1.

  Please refer to Chapter 42 (i.MX 6 PCI Express Root Complex Driver) of

"i.MX_6_Linux_Reference_Manual.pdf" in Linux documentation.

2.

  You may try using the recent (L3.10.53) Linux BSP.

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&appType=license&loca...

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_LINUX_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

3.

  The following thread may be useful.

“i.MX6Q PCIe EP/RC Validation System”


https://community.freescale.com/docs/DOC-95014


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,232 次查看
Yuri
NXP Employee
NXP Employee

1.

  Please refer to Chapter 42 (i.MX 6 PCI Express Root Complex Driver) of

"i.MX_6_Linux_Reference_Manual.pdf" in Linux documentation.

2.

  You may try using the recent (L3.10.53) Linux BSP.

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&appType=license&loca...

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_LINUX_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

3.

  The following thread may be useful.

“i.MX6Q PCIe EP/RC Validation System”


https://community.freescale.com/docs/DOC-95014


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复