How to enable PCI-e interface for SABRESD with Linux rel_imx_3.10.17_1.0.2_ga?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable PCI-e interface for SABRESD with Linux rel_imx_3.10.17_1.0.2_ga?

ソリューションへジャンプ
2,268件の閲覧回数
phanthavongdoua
NXP Employee
NXP Employee
0 件の賞賛
返信
1 解決策
1,948件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

  Please refer to Chapter 42 (i.MX 6 PCI Express Root Complex Driver) of

"i.MX_6_Linux_Reference_Manual.pdf" in Linux documentation.

2.

  You may try using the recent (L3.10.53) Linux BSP.

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&appType=license&loca...

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_LINUX_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

3.

  The following thread may be useful.

“i.MX6Q PCIe EP/RC Validation System”


https://community.freescale.com/docs/DOC-95014


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,949件の閲覧回数
Yuri
NXP Employee
NXP Employee

1.

  Please refer to Chapter 42 (i.MX 6 PCI Express Root Complex Driver) of

"i.MX_6_Linux_Reference_Manual.pdf" in Linux documentation.

2.

  You may try using the recent (L3.10.53) Linux BSP.

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_iMX6QDLS_Bundle&appType=license&loca...

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_LINUX_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

3.

  The following thread may be useful.

“i.MX6Q PCIe EP/RC Validation System”


https://community.freescale.com/docs/DOC-95014


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信