How to enable Dynamic Linux kernel debug info on imx8mp EVK board ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable Dynamic Linux kernel debug info on imx8mp EVK board ?

5,523件の閲覧回数
hit100
Contributor I

I am trouble shoot a clock driver issue on my customized board, which is ported from imx8mp ddr4 EVK board, but i have trouble to enable it , as by following the set up explained here, url https://www.ti.com.cn/content/dam/videos/external-videos/2/3816841626001/5399373110001.mp4/subassets...

CONFIG_DEBUG_FS=y
CONFIG_DEBUG_FS_ALLOW_ALL=y
# CONFIG_DEBUG_FS_DISALLOW_MOUNT is not set
# CONFIG_DEBUG_FS_ALLOW_NONE is not set

I always don't have the dynamic debug folder under my  /sys/kernel folder,

and here is the config , please tell me which is missing ? Thanks

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

5,444件の閲覧回数
_angelo_
Contributor III
what about checking
CONFIG_DYNAMIC_DEBUG=y ?
0 件の賞賛
返信

5,437件の閲覧回数
hit100
Contributor I

@_angelo_ 

CONFIG_DYNAMIC_DEBUG=y  has been confirmed what else missing here?

Regards

0 件の賞賛
返信

5,479件の閲覧回数
_angelo_
Contributor III

of course, you have to mount "debugfs"

 

mount -t debugfs none /sys/kernel/debug

and then access that directory

Also, if your driver is not probed, check driver compatible field to be the same you have in devicetree node.

Regards
Angelo Dureghello

 

0 件の賞賛
返信

5,472件の閲覧回数
hit100
Contributor I

Thanks Angelo,

 

Sorry for the confusion, actually my debug FS has been mounted, i have the folder /sys/kernel/debug 

but I  don't  have the subfolder of  "dynamic debug" under the folder /sys/kernel/debug , here is the layout of the debug folder

=================================

ls /sys/kernel/debug/
allocators debug_enabled extfrag mmc1 regulator usb
asoc devfreq fault_around_bytes mmc2 remoteproc v4l2-async
audio_pll_monitor device_component gc opp sleep_time wakeup_sources
bdi devices_deferred gpio phy split_huge_pages
block dma_buf hid pinctrl stmmaceth
bluetooth dma_pools ieee80211 pm_genpd suspend_stats
cec dmaengine iio pwm swiotlb
clk dri memblock regmap ufshcd

 

0 件の賞賛
返信

5,481件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you build the kernel the folder may be there.

Regards

0 件の賞賛
返信

5,458件の閲覧回数
hit100
Contributor I

screen shot for target board debug FSscreen shot for target board debug FS

Hi, 

Yes, the file system I provided is on target board file system here is the screen shot of that /sys/kernel/debug/ folder

still I can not see the "dynamic control? subfolder here 

 

Regards

 

0 件の賞賛
返信