Hi NXP Team
OS : Yocto 2.1 Board : imx6q sabresd
Our Customer need to add customer logo in Kernel.
And Display is VGA Port.
How to do display customer LOGO in VGA display in imx6q Yocto2.1?
Thanks.
已解决! 转到解答。
I didn't find 'config_ipu_di_clk' in the uboot source code, this should be the bsp source code difference, you need change it according to the error message, this should debug by yourself, you can compare the uboot source code between these two versions
Hi @joanxie
Our platfrom OS is Yocto 2.1_ 4.1.15_2.0.0.
The uboot version is different with your patch version.
Your patch file version is nxp/imx_v2015.04_4.1.15_1.0.0_ga.
We try the NXP demo board source code version (nxp/imx_v2016.03_4.1.15_2.0.0_ga in github).
The uboot version is different with v2015 and v2016 .
We get some error message. (It's can not patch success.)
Do you have any advice?