How to do display customer LOGO in VGA display ( imx6q Yocto2.1)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to do display customer LOGO in VGA display ( imx6q Yocto2.1)?

ソリューションへジャンプ
3,510件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

OS : Yocto 2.1   Board : imx6q sabresd

Our Customer need to add customer logo in Kernel.

And Display is VGA Port.

How to do display customer LOGO in VGA display in imx6q Yocto2.1?

Thanks.

ラベル(3)
0 件の賞賛
返信
1 解決策
3,343件の閲覧回数
charleshuang
Senior Contributor II

Hi @joanxie 

Thanks form you help and I have solution and provide my customer.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,498件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3,479件の閲覧回数
charleshuang
Senior Contributor II

Hi joanxie,

 

U-Boot build errors occur after I use "L4.1.15_GA1.2.0_uboot_logo_keep_patch_2017-01-06.zip".

It is important to note that our customer version is 4.1.15_2.0.0.

Do you have any suggestion about this issue ?

You can refer to the attachment for error logs.

Thank you.

0 件の賞賛
返信
3,468件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I didn't find 'config_ipu_di_clk' in the uboot source code, this should be the bsp source code difference, you need change it according to the error message, this should debug by yourself, you can compare the uboot source code between these two versions

"https://github.com/nxp-imx/uboot-imx/blob/nxp/imx_v2016.03_4.1.15_2.0.0_ga/arch/arm/cpu/armv7/mx6/cl..."

0 件の賞賛
返信
3,417件の閲覧回数
charleshuang
Senior Contributor II

Hi @joanxie 

Our platfrom OS is Yocto 2.1_ 4.1.15_2.0.0.

The uboot version is different with your patch version.

Your patch file version is nxp/imx_v2015.04_4.1.15_1.0.0_ga.

We try the NXP demo board source code version  (nxp/imx_v2016.03_4.1.15_2.0.0_ga in github).

The uboot version is different with  v2015 and v2016 .

We get some error message.  (It's can not patch success.)

Do you have any advice?

 

charleshuang_0-1690794429674.png

 

0 件の賞賛
返信
3,390件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

the patch is just for reference, if your version isn't the same one, you need refer to the patch, then modify the source code by yourself according to the patch

0 件の賞賛
返信
3,344件の閲覧回数
charleshuang
Senior Contributor II

Hi @joanxie 

Thanks form you help and I have solution and provide my customer.

 

 

0 件の賞賛
返信