How to do display customer LOGO in VGA display ( imx6q Yocto2.1)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to do display customer LOGO in VGA display ( imx6q Yocto2.1)?

跳至解决方案
3,362 次查看
charleshuang
Senior Contributor II

Hi NXP Team

OS : Yocto 2.1   Board : imx6q sabresd

Our Customer need to add customer logo in Kernel.

And Display is VGA Port.

How to do display customer LOGO in VGA display in imx6q Yocto2.1?

Thanks.

标签 (3)
0 项奖励
回复
1 解答
3,195 次查看
charleshuang
Senior Contributor II

Hi @joanxie 

Thanks form you help and I have solution and provide my customer.

 

 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,350 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复
3,331 次查看
charleshuang
Senior Contributor II

Hi joanxie,

 

U-Boot build errors occur after I use "L4.1.15_GA1.2.0_uboot_logo_keep_patch_2017-01-06.zip".

It is important to note that our customer version is 4.1.15_2.0.0.

Do you have any suggestion about this issue ?

You can refer to the attachment for error logs.

Thank you.

0 项奖励
回复
3,320 次查看
joanxie
NXP TechSupport
NXP TechSupport

I didn't find 'config_ipu_di_clk' in the uboot source code, this should be the bsp source code difference, you need change it according to the error message, this should debug by yourself, you can compare the uboot source code between these two versions

"https://github.com/nxp-imx/uboot-imx/blob/nxp/imx_v2016.03_4.1.15_2.0.0_ga/arch/arm/cpu/armv7/mx6/cl..."

0 项奖励
回复
3,269 次查看
charleshuang
Senior Contributor II

Hi @joanxie 

Our platfrom OS is Yocto 2.1_ 4.1.15_2.0.0.

The uboot version is different with your patch version.

Your patch file version is nxp/imx_v2015.04_4.1.15_1.0.0_ga.

We try the NXP demo board source code version  (nxp/imx_v2016.03_4.1.15_2.0.0_ga in github).

The uboot version is different with  v2015 and v2016 .

We get some error message.  (It's can not patch success.)

Do you have any advice?

 

charleshuang_0-1690794429674.png

 

0 项奖励
回复
3,242 次查看
joanxie
NXP TechSupport
NXP TechSupport

the patch is just for reference, if your version isn't the same one, you need refer to the patch, then modify the source code by yourself according to the patch

0 项奖励
回复
3,196 次查看
charleshuang
Senior Contributor II

Hi @joanxie 

Thanks form you help and I have solution and provide my customer.

 

 

0 项奖励
回复