Hello,
Could you please tell me how to display video captured by the OS08A20 camera via HDMI(LT8912)?
GST_DEBUG=3 gst-launch-1.0 v4l2src device=/dev/video0 ! "video/x-raw,width=1920,height=1080,format=YUYV" ! videoconvert ! autovideosink
■ Result
0:00:00.083718541 916 0xaaaaf3247f20 ERROR GST_PIPELINE grammar.y:1138:gst_parse_perform_link: could not link v4l2src0 to videoconvert0, neither element can handle caps video/x-raw, width=(int)1920, height=(int)1080, format=(string)YUYV WARNING: erroneous pipeline: could not link v4l2src0 to videoconvert0, neither element can handle caps video/x-raw, width=(int)1920, height=(int)1080, format=(string)YUYV
If any additional information is needed, please let me know.
Thank you in advance!
Thank you for your response.
The box is labeled as follows:
iMX95 Verdin EVK V1.1D
PN: 05241103
SN: 36204509
The board itself is labeled as follows:
iMX95 Verdin EVK CB V1.3A
PN:05211300
SN:35873003
best regards
Thank you for your response.
The box is labeled as follows:
iMX95 Verdin EVK V1.1D
PN: 05241103
SN: 36204509
The board itself is labeled as follows:
iMX95 Verdin EVK CB V1.3A
PN:05211300
SN:35873003
best regards
I tried to capture an image using v4l2-ctl, then the kernel crashed.
When I try to start a video capture using the following command, the kernel crashes (Oops) every time.
v4l2-ctl -d /dev/video0 --stream-mmap=1 --stream-count=1
Internal error: Oops: 0000000096000004 [#1] PREEMPT SMP
CPU: 1 PID: 691 Comm: v4l2-ctl Not tainted 6.6.23-lts-next-06236-gb586a521770e #1
Hardware name: NXP i.MX95 19X19 board (DT)
pc : formatter_subdev_enable_streams+0xb0/0x22c
...
Call trace:
formatter_subdev_enable_streams+0xb0/0x22c
v4l2_subdev_enable_streams+0xe4/0x268
mxc_isi_crossbar_enable_streams+0x12c/0x1d0
v4l2_subdev_enable_streams+0xe4/0x268
mxc_isi_pipe_enable+0x204/0x2ac
mxc_isi_vb2_start_streaming+0xa0/0xe4
vb2_start_streaming+0x68/0x15c
vb2_core_streamon+0xf8/0x1bc
vb2_streamon+0x18/0x64
mxc_isi_video_streamon+0x28c/0x314
v4l_streamon+0x24/0x30
__video_do_ioctl+0x32c/0x3f8
The media graph is active with crossbar/csi/formatter/ISI routing.
(See attached details below. media-ctl.txt)
...