How to disable Video Acceleration Unit and GPU in iMX8MQuad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable Video Acceleration Unit and GPU in iMX8MQuad

2,384件の閲覧回数
harshitshah
Contributor III

Hi NXP Team,

We are working on the development board set up with the iMX8MQuad chipset. However, we don't require the Video Acceleration unit and GPU as of now and we want to disable the same to save the power consumption.

Please provide the steps through which we can disable the i.MX8MQuad chipset through u-boot and kernel.

1) Video acceleration which includes 4Kp60, h.265 and VP9

2) GPUs 

We are checking the differences based on this link. https://www.nxp.com/docs/en/fact-sheet/i.MX8M-FS.pdf  

We are using the same Linux kernel 5.4 provided by NXP team.

Regards.

0 件の賞賛
返信
1 返信

2,334件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the enclosed file, find the chapter 5.1.8 Menu Configuration Options and chapter 6.7.3 Menu Configuration Options, you don't need to enable in the kernel configuration

0 件の賞賛
返信