How to defined a ripple range and absolute maximum voltage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to defined a ripple range and absolute maximum voltage?

Jump to solution
3,034 Views
t-iishii
Contributor II

Hi

I have some question about definition of ripple range.

It is defined 5% Vp-p of supply voltage average value in Hardware Development Guide.

If VDD_ARM_CAP  average value is 1.27V, ripple spec allowed 1.238V( = 1.27x0.975) ~ 1.301V( = 1.27x1.025).

Is it correct?

If so,

Absolute maximum voltages of VDD_ARM_CAP is defined to 1.3V in Datasheet.

Is it OK that average value is 1.27V of VDD_ARM_CAP because average value is less than 1.3V?

Or is it NG because top of ripple voltage is over a 1.3V?

Best regards,

Ishii.

Labels (2)
0 Kudos
Reply
1 Solution
2,893 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

1.27V+-0.0635V (allowed 5%) should be within allowed by datasheet range.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,894 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

1.27V+-0.0635V (allowed 5%) should be within allowed by datasheet range.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,893 Views
t-iishii
Contributor II

Dear igor

Thank you for your quick reply.

How about Absolute Maximum Ratings.

Is it applies an average value (i.e. 1.27V)?

Or average value + ripple (1.27V + 0.0653)?

Best regards,

Ishii.

0 Kudos
Reply
2,893 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

average value + ripple

Best regards
igor

0 Kudos
Reply
2,893 Views
t-iishii
Contributor II

Dear igor

Thank you for your quick response.

I understand a spec definition of datasheet.

Best regards,

Ishii.

0 Kudos
Reply