How to configure the cfg.init file for the mfg tool for imx6soloX sabre board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure the cfg.init file for the mfg tool for imx6soloX sabre board?

1,331 Views
soumyasatheesh
Contributor II

i am trying to burn the linux images to the sd card of the sabre board.How to configure the cfg.init file ? what are the parameters to be taken care of while configuring it?how it the parameter dependency on the vbscript?

Labels (1)
0 Kudos
Reply
2 Replies

1,222 Views
soumyasatheesh
Contributor II

but sir, there are 2  vbs files one has a prefix  of 1.2g which I didn't understand what it is?i am attaching screenshot  the vbs scripts2017-01-09_16h54_22.png

0 Kudos
Reply

1,222 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soumya

parameters for cfg.ini are taken from vbs file, just click on vbs file and

mfg tools automatically runs with parameters from that vbs file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------