How to configure the cfg.init file for the mfg tool for imx6soloX sabre board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure the cfg.init file for the mfg tool for imx6soloX sabre board?

1,375 次查看
soumyasatheesh
Contributor II

i am trying to burn the linux images to the sd card of the sabre board.How to configure the cfg.init file ? what are the parameters to be taken care of while configuring it?how it the parameter dependency on the vbscript?

标签 (1)
0 项奖励
回复
2 回复数

1,266 次查看
soumyasatheesh
Contributor II

but sir, there are 2  vbs files one has a prefix  of 1.2g which I didn't understand what it is?i am attaching screenshot  the vbs scripts2017-01-09_16h54_22.png

0 项奖励
回复

1,266 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soumya

parameters for cfg.ini are taken from vbs file, just click on vbs file and

mfg tools automatically runs with parameters from that vbs file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------