How to configure lpuart4 with the correct pads in the device tree for IMX93?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure lpuart4 with the correct pads in the device tree for IMX93?

跳至解决方案
732 次查看
LAAZIBI
Contributor II

I am trying to use uart4 with flow control(cts/rts) , I tried to add the Pin Multiplexing configuration for a qs93 board like you can see below: 

	pinctrl_uart4: uart4grp {
		fsl,pins = <
			MX93_PAD_GPIO_IO19__LPUART4_TX		0x31e
			MX93_PAD_GPIO_IO24__LPUART4_RX		0x31e
		>;
	};

	pinctrl_uart4_rtscts: uart4-rtsctsgrp {
		fsl,pins = <
			MX93_PAD_GPIO_IO26__LPUART4_CTS_B	0x31e
			MX93_PAD_GPIO_IO18__LPUART4_RTS_B	0x31e
		>;
	};


The Pad names seems to be not correct, known that I determine them from QS93 document, the pins I wanted to use are with the same GPIOs in the pad and for sure support the LPUART4 mentioned alternative functions. 

With these configuration, my recipe build fails with:

syntax error 
FATAL ERROR: Unable to parse input tree

 How can I determine the correct pad names in this case, or where I can find the correct definition if these pads? 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
724 次查看
LAAZIBI
Contributor II

My mistake was that I determined incorrectly the pad names from the documentation, here it is the correct configuration.  

	pinctrl_uart4: uart4grp {
		fsl,pins = <
			MX93_PAD_ENET2_TD0__LPUART4_TX		0x31e
			MX93_PAD_ENET2_RD0__LPUART4_RX		0x31e
		>;
	};

	pinctrl_uart4_rtscts: uart4-rtsctsgrp {
		fsl,pins = <
			MX93_PAD_ENET2_TD1__LPUART4_RTS_B	0x31e
			MX93_PAD_ENET2_RD2__LPUART4_CTS_B	0x31e
		>;
	};

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
725 次查看
LAAZIBI
Contributor II

My mistake was that I determined incorrectly the pad names from the documentation, here it is the correct configuration.  

	pinctrl_uart4: uart4grp {
		fsl,pins = <
			MX93_PAD_ENET2_TD0__LPUART4_TX		0x31e
			MX93_PAD_ENET2_RD0__LPUART4_RX		0x31e
		>;
	};

	pinctrl_uart4_rtscts: uart4-rtsctsgrp {
		fsl,pins = <
			MX93_PAD_ENET2_TD1__LPUART4_RTS_B	0x31e
			MX93_PAD_ENET2_RD2__LPUART4_CTS_B	0x31e
		>;
	};

 

0 项奖励
回复