I am trying to use uart4 with flow control(cts/rts) , I tried to add the Pin Multiplexing configuration for a qs93 board like you can see below:
pinctrl_uart4: uart4grp {
fsl,pins = <
MX93_PAD_GPIO_IO19__LPUART4_TX 0x31e
MX93_PAD_GPIO_IO24__LPUART4_RX 0x31e
>;
};
pinctrl_uart4_rtscts: uart4-rtsctsgrp {
fsl,pins = <
MX93_PAD_GPIO_IO26__LPUART4_CTS_B 0x31e
MX93_PAD_GPIO_IO18__LPUART4_RTS_B 0x31e
>;
};
The Pad names seems to be not correct, known that I determine them from QS93 document, the pins I wanted to use are with the same GPIOs in the pad and for sure support the LPUART4 mentioned alternative functions.
With these configuration, my recipe build fails with:
syntax error
FATAL ERROR: Unable to parse input treeHow can I determine the correct pad names in this case, or where I can find the correct definition if these pads?
Solved! Go to Solution.
My mistake was that I determined incorrectly the pad names from the documentation, here it is the correct configuration.
pinctrl_uart4: uart4grp {
fsl,pins = <
MX93_PAD_ENET2_TD0__LPUART4_TX 0x31e
MX93_PAD_ENET2_RD0__LPUART4_RX 0x31e
>;
};
pinctrl_uart4_rtscts: uart4-rtsctsgrp {
fsl,pins = <
MX93_PAD_ENET2_TD1__LPUART4_RTS_B 0x31e
MX93_PAD_ENET2_RD2__LPUART4_CTS_B 0x31e
>;
};
My mistake was that I determined incorrectly the pad names from the documentation, here it is the correct configuration.
pinctrl_uart4: uart4grp {
fsl,pins = <
MX93_PAD_ENET2_TD0__LPUART4_TX 0x31e
MX93_PAD_ENET2_RD0__LPUART4_RX 0x31e
>;
};
pinctrl_uart4_rtscts: uart4-rtsctsgrp {
fsl,pins = <
MX93_PAD_ENET2_TD1__LPUART4_RTS_B 0x31e
MX93_PAD_ENET2_RD2__LPUART4_CTS_B 0x31e
>;
};