Hi,
I'm using the imx8mm-lpddr4-evk board and following the "NXP Real Time Edge" Yocto build procedure
We are going to test the ethercat protocol for imx8mm board , so we followed the procedures from the "NXP Real Time Software user guide" to setup the master in the EVK board.
Following steps :
1. I've added the MAC address of the slave device to the /etc/ethercat.conf file in the master board.
However, the output of the ethercat master command shows that it's stuck at the "Waiting for device(s).." phase. How can I resolve this issue? We are only know the ethercat master seup but don't have the Slave setup.
When I run the command: $ ethercat master
The output I get is:
Master0
Phase: Waiting for device(s)..
Active: no
Slaves: 0
Ethernet devices:
Main: 00:1f:7b:1e:30:38 (waiting...)
Link: DOWN
Tx frames: 0
Tx bytes: 0
Rx frames: 0
Rx bytes: 0
Tx errors: 0
Tx frame rate [1/s]: 0 0 0
Tx rate [KByte/s]: 0.0 0.0 0.0
Rx frame rate [1/s]: 0 0 0
Rx rate [KByte/s]: 0.0 0.0 0.0
Common:
Tx frames: 0
Tx bytes: 0
Rx frames: 0
Rx bytes: 0
Lost frames: 0
Tx frame rate [1/s]: 0 0 0
Tx rate [KByte/s]: 0.0 0.0 0.0
Rx frame rate [1/s]: 0 0 0
Rx rate [KByte/s]: 0.0 0.0 0.0
Loss rate [1/s]: 0 0 0
Frame loss [%]: 0.0 0.0 0.0
Distributed clocks:
Reference clock: None
Application time: 0
2000-01-01 00:00:00.000000000
Can you please help us to resolve the issue?
Regards,
SanthanaKumarS