LTIB i.mx23 for ubuntu 20.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB i.mx23 for ubuntu 20.04

2,220件の閲覧回数
YavuzKaran
Contributor I

Hi,

What is the dowmload link of LTIB sofware imx23 for debian (ubuntu 20.04 or others one)

 

Best Regards

0 件の賞賛
返信
4 返答(返信)

2,206件の閲覧回数
YavuzKaran
Contributor I

Hi Igor,

when i press download option button inside your link page,open overview,documantation and hrdaware for buy.

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

where is the donload link ?

Regards

 

0 件の賞賛
返信

2,204件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

2,211件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi YavuzKaran

 

for i.MX23 ltib one can look at Archived Software and Documentation for the i.MX23 SDK Version 2009.12

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

Best regards
igor

0 件の賞賛
返信

1,577件の閲覧回数
Dhanyalakshmi
Contributor III

Hello,

I have followed below steps:

1. https://viaembedded.github.io/docs/vab820-hmi-dev/ltib.html followed this from chapter1 till chapter3 but when i executed ./ltib i got the result1.png file but i have installed all the packages.

2. Downloaded the source code from http://download.savannah.nongnu.org/releases/ltib/ latest version then executed ./ltib then i got the error which is in host_config.log file.In this i have a doubt that in host_config.log file i saw that rpc/rpc.h file is missing but in order to change the path from <rpc/rpc.h> to </usr/include/ntirpc/rpc/rpc.h> I'm not able to get in which file i need to change.

what is wrong and how to do it properly can you please suggest

タグ(1)
0 件の賞賛
返信