How to configure SSI1 in PCM mode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure SSI1 in PCM mode ?

1,504 Views
robinsingh
Contributor III

Hi All,

I am using Freescale Android BSP 4.4.3 ,kernel 3.10  on IMX6 Solo/Duallite . we have a custom board and want to interface with A BT/WIFI  module. Currenlty Wifi and Normal BT features are working for me and Audio over A2DP is also working. but we want to interface the Audio over PCM interface ( BT Module PCM interface connected to SSI1).

BT module is connected on AUDMUX 3 , So what will be the required changes for above approach ?

Is it possible to run SSI1 in PCM Mode ?

Thanks

Robin

Labels (3)
0 Kudos
Reply
1 Reply

1,281 Views
joanxie
NXP TechSupport
NXP TechSupport

SSI can support PCM(not pcm mode), for more detailed information, you can refer to the SSI chapter in the Reference Manual

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP

0 Kudos
Reply