Hi,
I am working on MX6q,use linux kernel 3.0.35.When I send data,use the oscilloscope to view CS signal,why I fill the ECSPIx_CONREG[BURST LENGTH] can only send 8 bits ,16 bits or 32 bits one time.Now I want to send more data one time,and the CS is low power, until the data is send, the CS is high power.
Hi,
I am field TXCNT in register ECSPIx_TESTREG, I am send 4 byte one time,I can catch waveform. As follows,
But, I can not catch the CS is low when send the 4 byte data. I am field TXCNT in register ECSPIx_TESTREG code, As follows,
Hi,
I can not find where avoid TX FIFO become empty.Can you show it to me ?
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi
to avoid CS go high one needs to make algorithm
in such way so avoid TX FIFO become empty untill
all bits will be sent.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------