Hello
I am using i.MX6ULL (Y2CVM08AB) and Nand flash which is W29N01HV, and the nand datasheet please refer to the attachment. According to the datasheet, I did that following configuration, but boot_cfg2 and boot_cfg4 , I have no idea, is there anyone can help me? thanks!
Boot Device CFG1 [7] CFG1 [6] CFG1 [5] CFG1 [4] CFG1 [3] CFG1 [2] CFG1 [1] CFG1 [0]
NAND - W29N01HV 1 0 0 1 0 0 0 1
Boot Device CFG2 [7 CFG2 [6 CFG2 [5 CFG2 [4 CFG2 [3 CFG2 [2 CFG2 [1 CFG2 [0
?
Boot Device CFG4 [7 CFG4 [6 CFG4 [5 CFG4 [4 CFG4 [3 CFG4 [2 CFG4 [1 CFG4 [0
?
Solved! Go to Solution.
Hi 国承 张
nand boot CFG settings are described in Table 8-10. NAND boot eFUSE descriptions
i.MX 6ULL Applications Processor Reference Manual
Specific for this nand configuration can be found on p.13 nand its datasheet:
1 block= 64 pages, BOOT_CFG1[5:4] - Pages in block
4-cycles (Figure 6-1 Array Organization) , BOOT_CFG1[1:0] - Row address cycles
other BOOT_CFG can be left at default settings.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks very much!
about Row address cycles I have some more questions.
4-cycles (Figure 6-1 Array Organization) , BOOT_CFG1[1:0] - Row address cycles,
do you means that BOOT_CFG1[1:0] is 10? not 01? 2-cycles?
thanks again for your confirmation.
seems you are right: Row address cycles = 2-cycles
Best regards
igor
OK, thanks igor!