How to check if it is a VBlank period

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to check if it is a VBlank period

1,302 次查看
zakio
Contributor I
I am using MIPI-DSI on i.MX 7Dual.
I'm trying to switch from HS mode to LP mode while drawing and read the registers on the LCD panel. I would like to do this during the Vblank period. Is there a way to check if it is during the Vblank period?
0 项奖励
回复
3 回复数

1,290 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zakio

 

>. Is there a way to check if it is during the Vblank period?

 

sorry this is not possible as LPDT (enter to LP mode) area is not within VSYNC as described in
Figure 13-36. Stable VFP Area Before Command Transfer Allowing Area

i.MX 7Dual Applications Processor Reference Manual

 

Best regards
igor

 

0 项奖励
回复

1,286 次查看
zakio
Contributor I

Hi igor

Thank you for your reply.
Does that mean I can't switch from HS mode to LP mode while drawing (from VSync to the next VSync)?
During the VBlank period, I'm thinking of stopping drawing and then switching.
 
Best regards
zakio
0 项奖励
回复

1,278 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Zakio

 

please refer to Figure 13-36. Stable VFP Area Before Command Transfer Allowing Area-

it shows area where it is possble:

"Only this area ..command through LPDT or HS (register configuration)"

 

i.MX 7Dual Applications Processor Reference Manual

 

Best regards
igor

0 项奖励
回复