How to check if hdmi is functioning ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check if hdmi is functioning ?

ソリューションへジャンプ
1,078件の閲覧回数
rans
Senior Contributor I

Hello,

Is there a way to check if hdmi output is functioning ?

We need to run qt application which display using hdmi, but I can't see how it works.

Another issue , is that I also don't understand which type of imx6 (solo/dual/etc) , I have... It is not mentioned in datasheet, and I can't see it being printed in boot, This is the boot log:

log.txt - Google Drive 

Thank you,

Ran

1 解決策
1,016件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ran

please try Demo Images from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

use Linux and Yocto Guides from linux doc package:

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,017件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ran

please try Demo Images from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

use Linux and Yocto Guides from linux doc package:

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------