How to check if hdmi is functioning ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to check if hdmi is functioning ?

Jump to solution
1,631 Views
rans
Senior Contributor I

Hello,

Is there a way to check if hdmi output is functioning ?

We need to run qt application which display using hdmi, but I can't see how it works.

Another issue , is that I also don't understand which type of imx6 (solo/dual/etc) , I have... It is not mentioned in datasheet, and I can't see it being printed in boot, This is the boot log:

log.txt - Google Drive 

Thank you,

Ran

1 Solution
1,569 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

please try Demo Images from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

use Linux and Yocto Guides from linux doc package:

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

please try Demo Images from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

use Linux and Yocto Guides from linux doc package:

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------