How to change the resolution of the screen?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the resolution of the screen?

3,224 Views
wangvictor
Contributor III

Hi All,

I'm using I.MX6 sabresd formy layer and qt wayland for my OS system.

I'm using 4.3 inch which the resolution is 480X272.

I've modify the dts file to match my panel.

my panel can show things out but with the wrong resolution.

I using below commend to see the resolution in my OS system.

cat /sys/devices/soc0/fb@0/graphics/fb0/modes

And It shows this to me.

800x480p-57

I don't know why it will happend?

I certainly sure that I'm giving 480X272 to my dts file.

Is that freescale cannot support the resolution(480X272)?

Or I have to setting anything else?

0 Kudos
Reply
1 Reply

2,249 Views
wangvictor
Contributor III

Finally, I found the solution.

In this file "linux-imx/4.1.15-r0/git/drivers/video/fbdev/mxc/mxc_lcdif.c" I have to redefined the default resolution of lcd.

Below is what I had modify.

#include "../../../../include/dt-bindings/panel/tm043.h"

.

.

.

static struct fb_videomode lcdif_modedb[] = {
#if 0
{
/* 800x480 @ 57 Hz , pixel clk @ 27MHz */
"CLAA-WVGA", 57, 800, 480, 37037, 40, 60, 10, 10, 20, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},
{
/* 800x480 @ 60 Hz , pixel clk @ 32MHz */
"SEIKO-WVGA", 60, 800, 480, 29850, 89, 164, 23, 10, 10, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},
#endif

{///*LCD winmate frank add 480x272 @ 60 Hz , pixel clk @ 9MHz */
DISP_NAME,PANEL_REFRESH,
PANEL_XRES, PANEL_YRES,
PANEL_PIXCLOCK,
PANEL_LEFT_MARGIN,
PANEL_RIGHT_MARGIN,
PANEL_UPPER_MARGIN,
PANEL_LOWER_MARGIN,
PANEL_HSYNC_LEN,
PANEL_VSYNC_LEN,
FB_SYNC_EXT,
FB_VMODE_NONINTERLACED,
0,},
};

"../../../../include/dt-bindings/panel/tm043.h" is the file that I add myself to defined different panel value.

0 Kudos
Reply