How to build and debug in Windows Qt ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build and debug in Windows Qt ?

2,560件の閲覧回数
huhyangjae
Contributor I

I am using imx6Q, the kernel version is 4.1.15, and the file system is Qt 5.8.0 in xwayland (krogoth version).

With ubuntu via vmware, you can build or debug with Qt.

But I would like to build and debug in Windows Qt. Windows currently has Qt creator 4.2.1 installed and Qt 5.8.0 installed.

You need a guide on how to set up the cross compiler, how to configure it, and how to build it.
If you have ever tried it, please give me a guide.

0 件の賞賛
返信
2 返答(返信)

2,437件の閲覧回数
dantx
Contributor I

The simplest way is via Toradex Easy Installer and the commercial version of Qt.

This works on a Windows or Ubuntu development system.

Have a look here: Partner Demo Image - Qt for Device Creation 

More details: Getting Started with Qt 

0 件の賞賛
返信

2,436件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the Section 8.4 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信