How to build and debug in Windows Qt ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build and debug in Windows Qt ?

2,632 次查看
huhyangjae
Contributor I

I am using imx6Q, the kernel version is 4.1.15, and the file system is Qt 5.8.0 in xwayland (krogoth version).

With ubuntu via vmware, you can build or debug with Qt.

But I would like to build and debug in Windows Qt. Windows currently has Qt creator 4.2.1 installed and Qt 5.8.0 installed.

You need a guide on how to set up the cross compiler, how to configure it, and how to build it.
If you have ever tried it, please give me a guide.

0 项奖励
回复
2 回复数

2,509 次查看
dantx
Contributor I

The simplest way is via Toradex Easy Installer and the commercial version of Qt.

This works on a Windows or Ubuntu development system.

Have a look here: Partner Demo Image - Qt for Device Creation 

More details: Getting Started with Qt 

0 项奖励
回复

2,508 次查看
art
NXP Employee
NXP Employee

Please refer to the Section 8.4 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复