How to build and debug in Windows Qt ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build and debug in Windows Qt ?

3,750 Views
huhyangjae
Contributor I

I am using imx6Q, the kernel version is 4.1.15, and the file system is Qt 5.8.0 in xwayland (krogoth version).

With ubuntu via vmware, you can build or debug with Qt.

But I would like to build and debug in Windows Qt. Windows currently has Qt creator 4.2.1 installed and Qt 5.8.0 installed.

You need a guide on how to set up the cross compiler, how to configure it, and how to build it.
If you have ever tried it, please give me a guide.

0 Kudos
Reply
2 Replies

3,627 Views
dantx
Contributor I

The simplest way is via Toradex Easy Installer and the commercial version of Qt.

This works on a Windows or Ubuntu development system.

Have a look here: Partner Demo Image - Qt for Device Creation 

More details: Getting Started with Qt 

0 Kudos
Reply

3,626 Views
art
NXP Employee
NXP Employee

Please refer to the Section 8.4 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply