Hello everyone,
After some research and a post on this forum, I'm asking this question : https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX93-EVK-flashing-problems-with-Linux-6-1-36-2-1-...
Is there a way to build a Yocto Linux Image for i.MX93 that is compatible with the silicon version A0?
Thanks for your support,
Louis
已解决! 转到解答。
Is there a way to precise I want the version 6.1.22_2.0.0 ?
> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below
Hello,
Thanks for you reply.
My goal is to have a package manager direclty on the Yocto Linux Image and both versions are fine I think.
If I'm right, in the conf/local.conf file in the Yocto build directory, I just need to add the following lines and build:
PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "packag-management"
Is there a way to precise I want the version 6.1.22_2.0.0 ?
Louis
Is there a way to precise I want the version 6.1.22_2.0.0 ?
> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below