How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

Jump to solution
2,074 Views
Louis3
Contributor II

Hello everyone,

 

After some research and a post on this forum, I'm asking this question : https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX93-EVK-flashing-problems-with-Linux-6-1-36-2-1-...

Is there a way to build a Yocto Linux Image for i.MX93 that is compatible with the silicon version A0?

 

Thanks for your support,

Louis

Labels (1)
0 Kudos
Reply
1 Solution
2,028 Views
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

View solution in original post

0 Kudos
Reply
3 Replies
2,045 Views
joanxie
NXP TechSupport
NXP TechSupport

do you need build A0 with 6.1.36? for A0 silicon, only supports 6.1.22

 

0 Kudos
Reply
2,040 Views
Louis3
Contributor II

Hello,

Thanks for you reply.

My goal is to have a package manager direclty on the Yocto Linux Image and both versions are fine I think.

If I'm right, in the conf/local.conf file in the Yocto build directory, I just need to add the following lines and build:

PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "packag-management"

 

Is there a way to precise I want the version 6.1.22_2.0.0 ?

 

Louis

0 Kudos
Reply
2,029 Views
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

0 Kudos
Reply