How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

跳至解决方案
1,953 次查看
Louis3
Contributor II

Hello everyone,

 

After some research and a post on this forum, I'm asking this question : https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX93-EVK-flashing-problems-with-Linux-6-1-36-2-1-...

Is there a way to build a Yocto Linux Image for i.MX93 that is compatible with the silicon version A0?

 

Thanks for your support,

Louis

标签 (1)
0 项奖励
回复
1 解答
1,907 次查看
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,924 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you need build A0 with 6.1.36? for A0 silicon, only supports 6.1.22

 

0 项奖励
回复
1,919 次查看
Louis3
Contributor II

Hello,

Thanks for you reply.

My goal is to have a package manager direclty on the Yocto Linux Image and both versions are fine I think.

If I'm right, in the conf/local.conf file in the Yocto build directory, I just need to add the following lines and build:

PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "packag-management"

 

Is there a way to precise I want the version 6.1.22_2.0.0 ?

 

Louis

0 项奖励
回复
1,908 次查看
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

0 项奖励
回复