How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build a compatible Yocto Linux image for i.MX93 (silicon v. A0) ?

ソリューションへジャンプ
1,862件の閲覧回数
Louis3
Contributor II

Hello everyone,

 

After some research and a post on this forum, I'm asking this question : https://community.nxp.com/t5/i-MX-Processors/NXP-i-MX93-EVK-flashing-problems-with-Linux-6-1-36-2-1-...

Is there a way to build a Yocto Linux Image for i.MX93 that is compatible with the silicon version A0?

 

Thanks for your support,

Louis

ラベル(1)
0 件の賞賛
返信
1 解決策
1,816件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,833件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you need build A0 with 6.1.36? for A0 silicon, only supports 6.1.22

 

0 件の賞賛
返信
1,828件の閲覧回数
Louis3
Contributor II

Hello,

Thanks for you reply.

My goal is to have a package manager direclty on the Yocto Linux Image and both versions are fine I think.

If I'm right, in the conf/local.conf file in the Yocto build directory, I just need to add the following lines and build:

PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "packag-management"

 

Is there a way to precise I want the version 6.1.22_2.0.0 ?

 

Louis

0 件の賞賛
返信
1,817件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

Is there a way to precise I want the version 6.1.22_2.0.0 ?

> I'm not sure if I understand this or not, if you need build the 6.1.22_2.0.0, you can find the document and prebuilt images from the link as below

"https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for..."

0 件の賞賛
返信