How to build UUT project (i.MX53) in Win XP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build UUT project (i.MX53) in Win XP?

ソリューションへジャンプ
1,510件の閲覧回数
dasmond
Contributor I

Hello,

Anyone have idea how to build UUT project in order to generate nk.nbo image ?

Thanks.

Regards,

Dasmond

ラベル(1)
0 件の賞賛
返信
1 解決策
1,340件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Please open the UUT pbxml file under osdesign like iMX53_ARD_UUT.pbxml, and then do sysgen.

It will build the nk.nb0 image under release folder.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,340件の閲覧回数
YixingKong
Senior Contributor IV

Dasmond, if your question had been answered, please click Correct Answer.

Thanks,

Yixing

1,341件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

Please open the UUT pbxml file under osdesign like iMX53_ARD_UUT.pbxml, and then do sysgen.

It will build the nk.nb0 image under release folder.

0 件の賞賛
返信