How to build UUT project (i.MX53) in Win XP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to build UUT project (i.MX53) in Win XP?

跳至解决方案
1,558 次查看
dasmond
Contributor I

Hello,

Anyone have idea how to build UUT project in order to generate nk.nbo image ?

Thanks.

Regards,

Dasmond

标签 (1)
0 项奖励
回复
1 解答
1,388 次查看
justin_jiang
NXP Employee
NXP Employee

Please open the UUT pbxml file under osdesign like iMX53_ARD_UUT.pbxml, and then do sysgen.

It will build the nk.nb0 image under release folder.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,388 次查看
YixingKong
Senior Contributor IV

Dasmond, if your question had been answered, please click Correct Answer.

Thanks,

Yixing

1,389 次查看
justin_jiang
NXP Employee
NXP Employee

Please open the UUT pbxml file under osdesign like iMX53_ARD_UUT.pbxml, and then do sysgen.

It will build the nk.nb0 image under release folder.

0 项奖励
回复